JAJSM76E December 2015 – August 2022 LMX2582
PRODUCTION DATA
The input signal noise scales by 20 × log(output frequency / input signal frequency), so always check this to see if the noise of the input signal scaled to the output frequency is close to the PLL in-band noise level. When that happens, the input signal noise is the dominant noise source, not the PLL noise floor.