JAJSMY5 July 2024
ADVANCE INFORMATION
Figure 6-1 shows the TRF1108 in an ac-coupled configuration with single 5V supply operation. The input common-mode voltage is internally set simplifying biasing of the device. The value of the ac-coupling capacitors at the inputs and output set the lower cutoff frequency for the gain. If the lowest signal frequency is 10MHz, use 100nF ac-coupling capacitors. If the lowest signal frequency is 9kHz, use a 4.7µF capacitor in parallel with 100nF capacitor on each input and output pin.