JAJSND3 December 2024 LM5125-Q1
ADVANCE INFORMATION
PIN | TYPE(1) | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
DLY | 1 | O | Average input current limit delay setting pin. A capacitor from DLY to AGND sets the delay from when VIMON reaches 1V until the average input current limit is enabled. |
SS | 2 | O | Soft-start time programming pin. An external capacitor and an internal current source set the ramp rate of the internal error amplifier reference during soft start. The device forces diode emulation during soft-start time. |
COMP | 3 | O | Output of the internal transconductance error amplifier. Connect the loop compensation components between the pin and AGND. |
AGND | 4 | G | Analog ground pin. Connect to the analog ground plane through a wide and short path. |
CSN1 | 5 | I | Current sense amplifier input of phase 1. The pin operates as the negative input pin. |
CSP1 | 6 | I | Current sense amplifier input of phase 1. The pin operates as the positive input pin. Input to the internal undervoltage lockout for the input voltage. |
VOUT | 7 | I | Output voltage sensing pin. An internal feedback resistor voltage divider is connected from the pin to AGND. Connect a 0.1μF local VOUT capacitor from the pin to ground. |
HO1 | 8 | O | High-side gate driver output for phase 1. Connect directly to the gate of the high-side N-channel MOSFET through a short, low inductance path. |
HB1 | 9 | P | High-side driver supply for bootstrap gate drive for phase 1. Boot diode is internally connected from VCC to the pin. Connect a 0.1μF capacitor between the pin and SW1. |
SW1 | 10 | P | Switching node connection for phase 1. Connect directly to the source of the phase 1 high-side N-channel MOSFET. |
LO1 | 11 | O | Low-side gate driver output for phase 1. Connect directly to the gate of the low-side N-channel MOSFET through a short, low inductance path. |
VCC | 12 | P | Output of the internal VCC regulator and supply voltage input of the internal MOSFET drivers. Connect a 10μF capacitor between the pin and PGND. |
PGND | 13 | G | Power ground connection pin for low-side gate drivers and VCC bias supply. |
LO2 | 14 | O | Low-side gate driver output for phase 2. Connect directly to the gate of the low-side N-channel MOSFET through a short, low inductance path. |
SW2 | 15 | P | Switching node connection for phase 2. Connect directly to the source of the phase 2 high-side N-channel MOSFET. |
HB2 | 16 | P | High-side driver supply for bootstrap gate drive for phase 2. Boot diode is internally connected from VCC to the pin. Connect a 0.1μF capacitor between the pin and SW2. |
HO2 | 17 | O | High-side gate driver output for phase 2. Connect directly to the gate of the high-side N-channel MOSFET through a short, low inductance path. |
BIAS | 18 | P | Supply voltage input to the VCC regulator. Connect a 1μF local BIAS capacitor from the pin to ground. |
UVLO/EN | 19 | I | Undervoltage lockout programming pin. The converter start-up and shutdown levels can be programmed by connecting this pin to the supply voltage through a resistor divider. If greater than VUVLO-RISING, phase 1 is enabled. |
CSP2 | 20 | I | Current sense amplifier input of phase 2. The pin operates as the positive input pin. |
CSN2 | 21 | I | Current sense amplifier input of phase 2. The pin operates as the negative input pin. |
RT | 22 | O | Switching frequency setting pin. The switching frequency is programmed by a single resistor between the pin and AGND. Switching frequency is dynamically programmable during operation. |
SYNCOUT | 23 | O | Clock output pin. SYNCOUT provides a phase shifted clock output, set by the CFG2.pin. SYNCOUT pin can be left floating when not used. |
SYNCIN | 24 | I | External clock synchronization pin. Input for an external clock that overrides the free-running internal oscillator. Connect the SYNCIN pin to ground when not used. |
CFG2 | 25 | I/O |
Device configuration pin. Sets if the device is configured as single, primary or secondary device using the internal or external clock and the Overvoltage Protection Level. |
CFG1 | 26 | I |
Device configuration pin. Sets the overvoltage protection level, spread spectrum mode, PGOOD configuration and 120% peak current limit latch off. |
CFG0 | 27 | I |
Device configuration pin. Sets the dead time and enables the 20μA ATRK current. |
PGOOD | 28 | O |
Power-good indicator with open-drain output stage. The pin is pulled low when the output voltage is less than the undervoltage threshold or great than the overvoltage threshold based on the CFG1-pin setting. The pin is also pulled low indicating faults (see Power-Good Indicator (PGOOD-pin)). The pin can be left floating if not used. |
MODE | 29 | I | Operation mode selection pin selecting DEM or FPWM. |
EN2 | 30 | I | Enable pin for phase 2. |
ILIM/IMON | 31 | O | Input current monitor and average input current limit setting pin. Sources a current proportional to phase 1 and phase 2 differential current sense voltage. A resistor is connected from this pin to AGND. |
ATRK/DTRK | 32 | I | Output regulation target programming pin. The output voltage regulation target can be programmed by connecting the pin through a resistor to AGND, or by controlling the pin voltage directly with a voltage in the recommended operating range of the pin from 0.2V to 2.0V. A digital PWM signal between 8% to 80% duty cycle sets the output voltage regulation in the recommended operating range. |
EP | - | G | Exposed pad of the package. The Exposed pad must be connected to AGND and soldered to a large ground plane to reduce thermal resistance. |