JAJSOA3B February 2023 – June 2024 TPS25948
PRODUCTION DATA
The TPS25948xx implements undervoltage protection on IN and OUT in case the applied voltage becomes too low for the system or device to properly operate. The undervoltage protection has a default lockout threshold of VUVP which is fixed internally. Also, the UVLO comparator on the EN/UVLO pin allows the undervoltage protection threshold to be externally adjusted to a user defined value. Figure 7-4 and Equation 1 show how a resistor divider can be used to set the UVLO set point for a given voltage supply.