JAJSP89 November 2024 LM5190
PRODUCTION DATA
Figure 7-4 shows the typical schematic diagram of a CC-CV buck regulator. In this example, the CV regulation target is 12V and the CC regulation target is 8A. Full-load efficiency is 95% at 48V input. The switching frequency is set at 400kHz by resistor RRT. The 12V output is connected to BIAS to reduce IC bias power dissipation and improve efficiency.
Depending on the source impedance of the input supply bus, an electrolytic capacitor can be required at the input to make sure of stability, particularly at low input voltage and high output current operating conditions. See Section 7.3 for more details.