JAJSRI9B October 2023 – June 2024 LM51772
PRODUCTION DATA
This over voltage protection monitors the voltage of the FB-pin and the int. feedback.
As this threshold is referenced to the programmed V(REF) the OVP1 is still working if one of the tracking features (e.g. DTRK or ATRK) has changed the Vo target value.
The converter maintains operatoin even the OVP1 threshold triggers.
The OVP1 is disabled during uSleep to avoid additional leakage current. The OVP1 signal gets masked that no fault is indicated from this signal during the uSleep operation.
This protection is disabled during the soft-start procedure and if the internal feedback is used instead of the ext. FB