JAJSSS6B January 2024 – June 2024 TPS7H3014-SP
PRODUCTION DATA
The TPS7H3014 incorporates four input channels to sequence/monitor up to four voltage rails. However, in the case where more than four channels are needed in the application, multiple devices can be daisy chained as needed. The daisy chain configuration is shown in Figure 8-15. In this case, only two devices are shown, however multiple IC can be configured as needed by the application.