JAJSSS6B January 2024 – June 2024 TPS7H3014-SP
PRODUCTION DATA
PIN | I/O(1) | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
SENSE1 | 1 | I | Non-inverting input of the comparator used to monitor the first rail to be sequenced up/down. To set the VON and VOFF voltages, connect an external resistive divider between the rail to be monitored and GND with the middle point tied to SENSE1. A voltage greater than 599mV (typ) on this pin is considered as a regulated voltage rail (VON). The VOFF is set by the IHYS current and the top resistor from the resistive divider. Refer to Top and Bottom Resistive Divider Design Equations. |
SENSE2 | 2 | I | Non-inverting input of the comparator used to monitor the second rail to be sequenced up/down. To set the VON and VOFF voltages, connect an external resistive divider between the rail to be monitored and GND with the middle point tied to SENSE2. A voltage greater than 599mV (typ) on this pin is considered as a regulated voltage rail (VON). The VOFF is set by the IHYS current and the top resistor from the resistive divider. Refer to Top and Bottom Resistive Divider Design Equations. |
SENSE3 | 3 | I | Non-inverting input of the comparator used to monitor the third rail to be sequenced up/down. To set the VON and VOFF voltages, connect an external resistive divider between the rail to be monitored and GND with the middle point tied to SENSE3. A voltage greater than 599mV (typ) on this pin is considered as a regulated voltage rail (VON). The VOFF is set by the IHYS current and the top resistor from the resistive divider. Refer to Top and Bottom Resistive Divider Design Equations. |
SENSE4 | 4 | I | Non-inverting input of the comparator used to monitor the fourth rail to be sequenced up/down. To set the VON and VOFF voltages, connect an external resistive divider between the rail to be monitored and GND with the middle point tied to SENSE4. A voltage greater than 599mV (typ) on this pin is considered as a regulated voltage rail (VON). The VOFF is set by the IHYS current and the top resistor from the resistive divider. Refer to Top and Bottom Resistive Divider Design Equations. |
REFCAP | 5 | O |
1.2V internal reference. Requires a 470nF external capacitor to GND. Do not load this pin. |
HYS | 6 | O | Hysteresis. Connect a 50kΩ resistor between this pin and GND, to program the hysteresis current (typically 24μA) at SENSE1 to SENSE4. Is recommended using a resistor with a 0.1% or better tolerance for hysteresis current accuracy. |
FAULT | 7 | O | FAULT. Open drain output which is forced low by the state machine to indicate an internally generated fault. Is recommended to pull-up this pin to VLDO with a 10kΩ resistor. However, a different external voltage source can be used as the pull-up as long as it is stable before commanding the sequence up and never drops below 1V during the operation of the device. |
UP | 8 | I | Non-inverting input of a comparator. A rising voltage greater than 599mV (typ) will induce a rising edge and will start a sequence up. This pin can be driven by an external controller, or connected to a main rail trough an external resistive divider with the middle point connected to the UP pin to start the sequence up automatically. This threshold has a fixed hysteresis of 100mV (typ). |
IN | 9 | I |
Input supply to the device. Input voltage range is from 3V to 14V. Connect at least a 0.1μF ceramic capacitor as close as possible to the pin. |
REG_TMR | 10 | I/O | Time to regulation timer. Connect a resistor to GND between 10.5kΩ and 1.18MΩ to set the allowed time for a SENSEx rail to reach the regulation threshold (VON). The delay can be adjusted from 0.25ms to 25ms. Leave this pin floating to deactivate this feature. |
DLY_TMR | 11 | I/O | Delay timer. Connect a resistor to GND between 10.5kΩ and 1.18MΩ to set the sequence up and down delay. The delay can be adjusted from 0.25ms to 25ms. Leave this pin floating for no delay. |
SEQ_DONE | 12 | O | Sequence done. Push-pull output with VOH level set by PULL_UP2 input supply voltage. Indicates when the sequence up or down is completed. |
PWRGD | 13 | O | Power Good. Push-pull output with VOH level set by PULL_UP2 input supply voltage. Indicates when all rails (SENSE1 to SENSE4 ) are in regulation (greater than VONx). |
GND | 14 | — | Ground. |
VLDO | 15 | O |
Output of internal regulator. Requires at least 1μF external ceramic capacitor to GND. Allowed loading of this regulator are: FAULT pull-up using a 10kΩ resistor or to turn-off unused channels by connecting directly to SENSE2 to SENSE4 as needed. |
DOWN | 16 | I | Non-inverting input of a comparator. A falling voltage lower than 498mV (typ) will induce a falling edge and will start a sequence down. This pin can be driven by an external controller, or connected to a main rail through an external resistive divider with the middle point connected to the DOWN pin to start the sequence down automatically. This threshold has a fixed hysteresis of 100mV (typ). |
PULL_UP2 | 17 | I | Input supply voltage to program the pull-up voltage for the push-pull output stage on SEQ_DONE and PWRGD. Connect at least a 1μF ceramic capacitor as close as possible to the pin. |
PULL_UP1 | 18 | I | Input supply voltage to program the global pull-up voltage for the push-pull output stages on EN1 to EN4. Connect at least a 1μF ceramic capacitor as close as possible to the pin. |
EN4 | 19 | O | Enable 4. Push pull output with VOH level set by the PULL_UP1 input supply voltage. Connect to the logic enable signal of the device to control and to be monitored by SENSE4. |
EN3 | 20 | O | Enable 3. Push pull output with VOH level set by the PULL_UP1 input supply voltage. Connect to the logic enable signal of the device to control and to be monitored by SENSE3. |
EN2 | 21 | O | Enable 2. Push pull output with VOH level set by the PULL_UP1 input supply voltage. Connect to the logic enable signal of the device to control and to be monitored by SENSE2. |
EN1 | 22 | O | Enable 1. Push pull output with VOH level set by the PULL_UP1 input supply voltage. Connect to the logic enable signal of the device to control and to be monitored by SENSE1. |
Thermal pad | — | Internally grounded. It is recommended to connect this metal thermal pad to a large ground plane for effective heat dissipation. | |
Metal lid | Lid | — | The lid is internally connected to the thermal pad and GND through the seal ring. |