JAJSTM8 April 2024 AFE20408
PRODUCTION DATA
The resistor string structure consists of a series of resistors, each of value R, as shown in Figure 6-2. The code loaded to the DAC determines at which node on the string the voltage is tapped off to be fed into the output amplifier. The voltage is tapped off by closing one or more of the switches connecting the string to the amplifier. This resistor string architecture has inherent monotonicity, voltage output, and low glitch.