JAJSTM8 April 2024 AFE20408
PRODUCTION DATA
The update mode for each DAC channel is determined by the value of the corresponding SYNCEN bit in the DAC_SYNC_CFG register (in the DAC Configuration Register page). In asynchronous mode, a write to the DAC buffer data register results in an immediate update of the DAC active register and DAC outputs. In synchronous mode, writing to the DAC data register does not automatically update the DAC output. Instead, the update occurs only after a DAC trigger event. A DAC trigger signal is generated either by setting the DAC_TRIG bit in the TRIGGER register (located in the global register page) or by the FLEXIO pin when configured as LDAC (the LDAC pin can only be used to trigger DACA0 and DACA2). The synchronous update mode enables simultaneous update of multiple DAC outputs.