JAJSTW1 August 2024 TPS55287-Q1
PRODUCTION DATA
The output current limit is implemented by putting a current sense resistor between the ISP and ISN pins along with setting a limit voltage between the ISP pin and the ISN pin through register 02h. The maximum value of the limit voltage between the ISP and ISN pins is 63.5mV. The default limit voltage is 50mV. The current sense resistor between the ISP and ISN pins should be selected to ensure that the output current limit is set high enough for output. The output current limit setting resistor is given by Equation 18.
where
Because the power dissipation is large, make sure the current sense resistor has enough power dissipation capability with large package.