JAJSUY7 May 2024 MCT8316A-Q1
PRODUCTION DATA
In closed loop operation, the MCT8316A-Q1 drives the motor using trapezoidal commutation. The commutation instant is determined by the BEMF zero crossing on the phase which is not driven (Hi-Z). The duty cycle of the applied motor voltage is determined by DUTY OUT (see SPEED Control).