JAJSVD3 September 2024 LMR51603-Q1
PRODUCTION DATA
The LMR51603-Q1 can also be used to replace asynchronous buck converters, which need a rectifying diode in the application circuit. The design works fine with or without a rectifying diode connected to the switch node of the LMR51603-Q1 as shown in Figure 8-2.