JAJSVI1 October 2024 TPS25763-Q1
PRODUCTION DATA
The TPS25763-Q1 has one internally fixed VIN UVLO and one user programmable UVLO using the EN/UVLO pin. Both thresholds must be cleared for the device to start up.
The EN/UVLO pin has three distinct voltage ranges: shutdown, standby, and operating. When the EN/UVLO pin is below the standby threshold VEN(STBY), the device is disabled in a low power shutdown. When EN/UVLO voltage is greater than the standby threshold VEN(STBY) but less than the operating threshold VEN(OPER), the internal bias rails, LDO_5V, LDO_3V3, and LDO_1V5 regulators are enabled but remaining device functions are disabled. When EN/UVLO is greater than the operating threshold VEN(OPER) and LDO_5V, LDO_3V3 and LDO_1V5 regulators are above their respective undervoltage threshold UVLO thresholds, the device is fully functional. The EN/UVLO pin includes fixed hysteresis between the shutdown mode and the standby mode.
EN/UVLO (1) | LDOs | DEVICE OPERATION |
---|---|---|
VEN/UVLO < VEN(LDO_V5V_F) | — | Shutdown: LDO_5V, LDO_3V3 and LDO_1V5 OFF. M0 (MCU) is OFF. |
VEN(LDO_V5V_R) < VEN/UVLO < VEN(STBY) | — | Standby: LDO_5V, LDO_3V3 and LDO_1V5 ON. M0 (MCU) is OFF. |
VEN/UVLO > VEN(OPER) | LDO_5V < VLDO_5V(UVLO_R), or LDO_3V3 < VLDO_3V3(UVLO_R); or LDO_1V5 < VLDO_1V5(UVLO_R) | LDO_5V, LDO_3V3 and LDO_1V5 ON, M0 (MCU) is OFF. |
VEN/UVLO > VEN(OPER) | LDO_5V > VLDO_5V(UVLO_R), and LDO_3V3 > VLDO_3V3(UVLO_R), and LDO_1V5 > VLDO_1V5(UVLO_R) | Operating: M0 (MCU) is ON. |
In some cases an input UVLO level different than that provided by the internal VIN(UVLO) is needed and can be accomplished by using the circuit shown in UVLO Threshold Programming. The input voltage at which the device turns on is designated VON; while the turnoff voltage is VOFF. First a value for RENB is chosen in the range of 13 kΩ to 22 kΩ. Use Equation 3 and Equation 7 to calculate RENT and VOFF.
The hysteresis between the UVLO turn-on threshold and turn-off threshold is set by the upper resistor in the EN/UVLO resistor divider and is given by:
Where
If the programmable UVLO is not required, the EN/UVLO pin can be connected to the IN pin with a 47 kΩ, or larger, resistor.