JAJSVI4 October 2024 ADS127L21B
PRODUCTION DATA
The device is also reset through SPI operation by inputting a long bit pattern. The input pattern is not part of the regular command format. CS must remain low for the entire bit sequence. There are two input patterns that can reset the ADC: pattern 1 and pattern 2. Pattern 1 consists of a minimum 1023 consecutive ones followed by one zero. The device resets on the falling edge of SCLK when the final zero is shifted in. This pattern is used for either 3- or 4-wire SPI modes. Figure 7-29 shows a pattern 1 reset example.
Reset pattern 2 is only used with the 4-wire SPI mode. To reset, input a minimum of 1024 consecutive ones (no ending zero value), followed by taking CS high, at which time reset occurs. Use pattern 2 when the devices are connected in daisy-chain mode. Figure 7-30 shows a pattern 2 reset example.