JAJSVI5 October 2024 DRV8376
ADVANCE INFORMATION
The current-limit circuit activates if the current flowing through the low-side MOSFET exceeds the ILIMIT current. This feature restricts motor current to less than the ILIMIT.
The current-limit circuitry utilizes the current sense amplifier output of the three phases compared with the voltage at ILIMIT pin. Figure 7-28 shows the implementation of current limit circuitry, the output of current sense amplifiers are combined with star connected resistive network. This measured voltage VMEAS is compared with the external reference voltage VILIMIT pin to realize the current limit implementation. The relation between current sensed on OUTX pin and VMEAS threshold is given as:
where
The ILIMIT threshold can be adjusted by configuring the voltage at ILIMIT pin. ILIMIT varies linearly between 0A to 4A, as the voltage at ILIMIT pin varies from VREF/2 to VMEAS. A voltage more than VREF/2 can be applied to disable ILIMIT.
Current limit comparator output is blanked for a blanking time, on every rising edge of high side and low side switch control input (INHx and INLx) and the DRV8376 output state depends on the INHx and INLx status during blanking time. The blanking time is configured through ILIM_BLANK_SEL in SPI device and the blanking time is fixed to 5.5 us for slew rate of 50 and 1.8us for all other slew rates in hardware variant.
When then the current limit activates, the high-side FET of each half bride is disabled until the rising edge of the high side (INHx) of that half bridge as shown in Figure 7-29. The low-side FETs can operate in brake mode or Coast (high-Z) mode by configuring the ILIM_MODE bit in the SPI device variant. The low-side FETs operate in Coast (high-Z) mode in the hardware variant.