Prepare two laptop computers: CCS is running on PC1. PC2 is used to control and monitor the PFC through a GUI HTTP page.
Make sure the hardware setup is the same with INCR_BUILD 4. Connect PC2 to Port J4 (Ethernet connector – RJ45 connector) of TMDSCNCD28388D control card using an ethernet cable.
Change the network setting of PC2 to enable static IP, configure it to 192.168.0.7 (anything other than 192.168.0.4 which is the IP Address of F2838x)