JAJU459B December 2017 – November 2022
The STO2 signal goes low for a period of 15 ms. As Figure 3-10 and Figure 3-11 show, the response time measured between the STO signal going low to the activation of the RDY pin is 7.4 ms. As the VCC2 goes below the UVLO threshold, the RDY pin is activated. The UVLO+ threshold for ISO5852S is 12 V. The response time is a function of the capacitance C7 at the output of the smart switch. Vary the response time by changing the value of capacitance.