JAJU459B December 2017 – November 2022
The safe-state is triggered by the following events:
Drive State Feedback STO_FB Subsystem
The STO_FB signal is an active low signal and indicates the drive state. A high signal (logic level 1) indicates normal drive operation, while a low signal (logic state 0) indicates the drive is in the safe state. The schematic is shown in Figure 2-5. The output signals STO_1_FB and STO_2_FB of the corresponding STO_1 and STO_2 safe subsystems are logically combined to a single active low feedback signal STO_FB through an isolated 24-V digital output. The corresponding logic states are shown in Table 2-3.
INPUT 1: STO_1 |
INPUT 2: STO_2 |
OUTPUT 1: STO_1_FB |
OUTPUT 2: STO_2_FB |
DRIVE STATE |
STO_FB |
COMMENT |
---|---|---|---|---|---|---|
1 |
1 |
1 |
1 |
Normal operation |
1 |
|
0 |
0 |
0 |
0 |
Safe state (off) |
0 |
|
1 |
1 |
0 |
1 (stuck high fault) |
Safe state (off) |
0 |
(1) The MCU has detected a single dangerous fault (stuck high) in subsystem STO_2 and has triggered the safe state through STO_1 subsystem. |
1 |
1 |
1 (stuck high fault) |
0 |
Safe state (off) |
0 |
(2) The MCU has detected a single dangerous fault (stuck high) in subsystem STO_1 and has triggered the safe state through STO_2 subsystem. |
0 |
0 |
0 |
1 |
Safe state (off) |
0 |
Single detected fault could be detected earlier already, see (1) in above row. |
0 |
0 |
1 (stuck high fault) |
0 |
Safe state (off) |
0 |
Single detected fault could be detected earlier already, see (2) in above row. |
0 |
0 |
1 (stuck high fault) | 1 (stuck high fault) | Normal operation |
1 |
Dangerous state, due to two dangerous faults, one in each safe subsystem STO_1 and STO_2. Note: The system is designed for single fault tolerance (HFT=1), but not two faults, one in each in each subsystem. |
The STO_FB signal can be active low (logic state 0), while both STO_1 and STO_2 are inactive high (logic state 1). This state occurs when the diagnostics MCU (SIL 1) detects a single dangerous fault in one of the STO_1 or STO_2 subsystems. If a short or stuck high was found, the MCU puts the 3-phase IGBT inverter into a safe state by driving both diagnostic pulses MCU_Diag_Ctrl_Out1 and MCU_Diag_Ctrl_Out2 continuously low. This state can be used for example by an external safety PLC to recognize a single fault in either STO_1 or STO_2 systems and take appropriate actions. The safety PLC and related action are out of scope for this design.