The DUT in this design is set up and is operated in several pieces:
- One TIDA-01606 power board
- Three TIDA-01606 gate driver cards
- One TIDA-01606 ISOHVCARD
- TMS320F28379D Control Card
- Mini USB cable
- One USB isolator
- Laptop or other computer
The test equipment required to power and evaluate the design is as follows:
- 24-V, 4-A bench style supply for primary board power
- For PFC Mode
- 400 VL-L
capable three-phase AC source
- > 10-kVA resistive load
to be connected at the DC output
- For Inverter Mode
- Star connected resistive load network like the 10-kW Simplex PowerStart load bank
- 800-V, 12-A power supply for DC link input
- Four-channel, power quality analyzer
- Oscilloscope, voltage meter, and current probes
The design follows an HSEC control card concept.
This design can be scaled across multiple devices from the C2000™ MCU
product family with a compatible HSEC control card. The key resources used for
controlling the power stage on the MCU are listed in Table 3-1.