JAJU680A January 2019 – July 2022
Different meters and transducers have different responses; consequently, it is important to characterize the frequency response of the meter to obtain an optimal performance.
The MSP430 Ultrasonic Sensor Design Center Tool GUI provided in this reference design can be used for this purpose. The GUI includes a Frequency Sweep panel. Ultrasonic Sensing Design Center User's Guide describes the detailed operation, but a brief description is provided here for completeness.
To start a sweep, do the following:
The Frequency Sweep tool helps to determine at which transducer excitation frequency the ADC capture achieves the maximum amplitude. The frequency at which the peak amplitude is reached should be used as the new F1 parameter to achieve the strongest signal for the meter configuration. For the example, in Figure 4-11 a value of 170 to 180 should be placed into the F1 parameter.