JAJU737A June   2019  – March 2020 AWR1243 , AWR2243

 

  1.   改訂履歴

Frame Based Beam Steering

In the subframe used for TX beamforming, the number of burst within this subframe is equal to the number of different desired angles (same as number of chirp configurations). Each burst is associated with each chirp configuration, so a burst is equivalent to a frame within which each chirp has the same phase shifter value. Figure 11 demonstrates the mechanism of frame based beam steering.

Figure 11. Frame Based Beam Steering TIDEP-01012 tidep-01012-frame-based-beam-steering-tiduen5.gif