JAJU785A January   2017  – March 2020

 

  1.   改訂履歴

Build and Load the Project

  1. Turn ON the 12-V auxiliary supply.
  2. If another lab option was built previously, right-click on the project name, and click on Clean Project. Click Project > Build All button, and watch the tools run in the build window.
  3. Click the Debug button (TIDM-1001 tidm-1001-for-section-4.2.2.3-inline-graphic.png) or click Run > Debug. The code should compile and load.
  4. Notice the CCS Debug icon in the upper corner, which indicates the Debug Perspective view. The program should be stopped at the start of main().