3.2.3.1.2.4 Debug Environment Windows
It is standard debug practice to watch local and global variables while debugging code. There are various methods for doing this in CCS, such as memory windows and watch windows. Additionally, CCS has the ability to make time (and frequency) domain plots, which allows the user to view waveforms using graph windows.
- Populate the Expressions Window entries by clicking View > Scripting console on the menu bar and then opening thesetupdebugenv_lab1.js file from the project directory using the scripting console Open File (
) command. The Expressions Window should look like Figure 24.
Table 4. Lab 1 Description of Expressions Window Entries
VARIABLE |
DESCRIPTION |
LLC_buildLevel |
Shows which lab is loaded. |
LLC_startFlag |
Set this variable to 1 to start the powerstage. |
LLC_vPri_Volts |
Input voltage in Volts. Only valid if jumper J15 is populated on the TIDM-1001 board. |
LLC_iPri_PH1_Amps |
The primary tank current in phase 1 in Amps. |
LLC_iPri_PH2_Amps |
The primary tank current in phase 2 in Amps. |
LLC_iSec_Amps |
Secondary (output) current in Amps. |
LLC_periodRef_debug_pu |
The variable used to control the switching period in lab 1. It is in per unit format. |
LLC_dutySet_PH1_debug_pu |
The variable used to control the switching duty for phase 1. It is in per unit format. |
LLC_dutySet_PH2_debug_pu |
The variable used to control the switching duty for phase 2. It is in per unit format. |