JAJU791 April 2020
If LED driver has changes based on different LED specifications or even Lasers, you can use LED Driver Components Calculator. LED driver components calculator is an excel-based calculator that allows customers to calculate various components values based on led driver specifications in tab Component Values. You can enter values in blue such as LED voltage signal, LED current and others, and the calculator will calculate the rest of the values needed for the driver to work as shown in Figure 12.
Second tab ComponentRatings tab shown in Figure 13 calculates various component ratings based on selected specs from ComponentValues tab. This should help customers choose appropriate power and voltage ratings.