JAJU793 October 2020
Over voltage clamping mode is implemented by shorting together the j 1 connector. By doing so the OV pin will be connected to the resistor divider which is connected to the source of the HGATE driven MOSFETs.
Figure 3-2 shows over-voltage clamping with the HGATE MOSFETs switching to regulate the output. By having the OV pin connected to the resistor divider at the source of the HGATE driven MOSFETs, the MOSFETs will switch on and off clamping the voltage at the output.