JAJU802A January 2022 – October 2022
The sensorless FOC structure for an IPMSM is illustrated in Figure 2-16. In this system, the eSMO is used for achieving the sensorless control an IPMSM system, and the eSMO model is designed by utilizing the back EMF model together with a PLL model for estimating the rotor position and speed.
An IPMSM consists of a three-phase stator winding (a, b, c axes), and permanent magnets (PM) rotor for excitation. The motor is controlled by a standard three-phase inverter. An IPMSM can be modeled by using phase a-b-c quantities. Through proper coordinate transformations, the dynamic PMSM models in the d-q rotor reference frame and the α-β stationary reference frame can be obtained. The relationship among these reference frames are illustrated in Equation 46. The dynamic model of a generic PMSM can be written in the d-q rotor reference frame as:
Where and are the q-axis and d-axis stator terminal voltages, respectively; and are the d-axis and q-axis stator currents, respectively; and are the q-axis and d-axis inductances, respectively, p is the derivative operator, a short notation of ; is the flux linkage generated by the permanent magnets, is the resistance of the stator windings; and is the electrical angular velocity of the rotor.
By using the inverse Park transformation as shown in Figure 2-17, the dynamics of the PMSM can be modeled in the α-β stationary reference frame as:
Where the and are components of extended electromotive force (EEMF) in the α-β axis and can be defined as: