JAJU802A January 2022 – October 2022
There are high voltages present on the board. To safely evaluate this board, use an appropriate isolated and current limited power source. Before power is applied to the board, an appropriate resistive or electronic load must be connected at the output. Do not handle the unit when power is applied to it. Only use appropriately rated equipment and follow proper isolation and safety practices.
Use caution when connecting scopes and other test equipment to the board because the AC rectifier generates the DC-output voltage, which has a HOT Ground floating from the protective earth ground. Isolation transformers must be used when connecting grounded equipment to the Kit.