JAJU802A January 2022 – October 2022
The current sensing circuit is used to convert the PFC inductor current signal into low voltage signal, and then to condition the sensed signal to meet the requirements of the ADC input port. As part of IPFC inner current loop control, AC current sensing is crucial. To do that, this design perform current sensing on returning point to diode bridge. It is rectified version of AC current. This method offers the benefit of current sensing with respect to system ground. There are two parts in the current sensing circuit as shown in Figure 2-4:
Recommended voltage across shunt resistor is decided as 0.2 to 0.25 V to optimize the power dissipation and better noise performance. Power dissipation across shunt has been limited to less than 0.05% of total power Exact value of full scale voltage is trial and error value depend on standard Shunt resistor available
Where Gi = 4.892 as show in Figure 2-4