JAJU804D August 2022 – December 2022
For this step, use a target configuration file that erases the entire Flash. Refer to Figure 3-2 for details.
At this point, the custom bootloader is programmed on Flash bank 0 and the application is programmed on Flash bank 1.
For this step, use a target configuration file that erases only the necessary sectors, not the entire Flash. Refer to Figure 3-3 for details.