JAJU808 July 2021
As Figure 2-1 and Figure 2-2 illustrate, the TIDA-010197 reference design is comprised of numerous subsystems including:
The ability to monitor voltage, current, and temperature has multiple value propositions, and is critical for maintaining reliable system operation in many applications. From a system health perspective, the ability to have accurate voltage, current, and temperature data for a board is an effective and relatively simple approach to get a relative metric on the health of a board. Changes in current, voltage, and temperature over time could indicate failure, or potential for failure, of some components. Another use case is operation with sensitive components such as many power amplifiers or thermoelectric coolers. The MCU monitors the current, voltage, or temperature (or all of these) of the power amplifier or thermoelectric cooler and triggers a recalibration if there is a deviation over a preset threshold at which a calibration was performed.
There are two variations of the signal chain. Details on the differences are found in the systems overview (Section 2.1).
To power the TIDA-010197 reference design, there are two methods. The first method provides 5 V and 12 V from an external power supply. The other option supplies a single 5-V rail and utilizes the unregulated boost with LDO.