To test the current monitoring
circuits, a power supply and electronic load are required. The power supply
provides a voltage on one side of the sense resistor, and the other side of the
sense resistor is connected to the electronic load. For the ±2 A and 0.25–1 A
monitoring, two tests are performed for each rail. All tests were done at an ambient
temperature of 25°C.
The following list provides the test
procedure for Noise floor:
- Short both sides of the sense
resistor to ground.
- Open Code Composer Studio (CCS)
to run the MSP430 software.
- Configure the MSP430 software for
either internal or external ADC, and set the desired ADC channel.
- Capture and plot 1000 plots by
using memory export and Microsoft Excel to convert the digital data to the ADC
voltage reading using the ADC conversion equation.
- Calculate the actual current
reading by solving the linear equation
Equation 8.
- Repeat for the rest of the other
current inputs.
The following
list provides the test procedure for Linearity
- Connect the power supply to the
desired terminal block as shown in Figure 3-3.
- Open CCS to run the MSP430
software.
- Configure the MSP430 software for
either internal or external ADC, and set the desired ADC channel.
- Capture and export 1000
measurements by using the memory export and Microsoft Excel to convert the
digital data to the voltage reading using the ADC conversion equation.
- Calculate the actual current
reading by solving the linear equation:
Equation 9.
- Repeat over the rest of the
current range.