JAJU819B April 2021 – June 2021
Figure 4-1 shows key hardware components. This hardware uses the kit of Bidirectional 400-V/12-V DC/DC Converter Reference Design as the base board and with some modification for peak current mode control.
The key signal connections between the controlCARD and the base board are listed in the Table 4-1
SIGNAL NAME |
DESCRIPTOIN |
CONNECTION TO CONTROLCARD |
---|---|---|
ePWM-1A | PWM drive for full-bridge switch Q2 | GPIO-00 |
ePWM-1B | PWM drive for full-bridge switch Q3 | GPIO-01 |
ePWM-2A | PWM drive for full-bridge switch Q1 | GPIO-02 |
ePWM-2B | PWM drive for full-bridge switch Q4 | GPIO-03 |
ePWM-4A | PWM drive for sync rectifier/push-pull switch Q6 | GPIO-07 |
ePWM-4B | PWM drive for sync-rectifier/push-pull switch Q5 | GPIO-06 |
VLV-FB | Low voltage bus – voltage feedback | ADC-A0 |
ILV-FB | Low voltage current feedback (Jumper J2 populated) | ADC-B3/COMP2A |
ILV-FILT | Heavily filtered low voltage current feedback | ADC-B2 |
VHV-FB | High voltage bus – voltage feedback | ADC-B1 |
IHV-FB | Transformer high voltage winding current | ADC-A2/COMP1A |
IHV-FILT | Heavily filtered transformer high voltage winding current | ADC-A1 |
This board provides a lot of jumper options for experimentation but there are some jumpers that must be populated for proper operation of the board. These jumpers that must be populated are listed below:
C:JPG1, E:JPG1, J2, J5, J6, J7, J8, J10, J11, J12, J13, J15, J16, and J19.
Some hardware modifications are required by the customer before running the reference code in this board.
Notes: Some magnetic components in the original board are replaced for peak current mode control as shown in Table 4-2.
CURRENT | ORIGINAL | |
---|---|---|
Main transformer | MPS P6524_A | VITEC AF5551R |
Secondary side inductor | VITEC 6193R | VITEC AF5666BR |
Shim inductor | VITEC 6194R | VITEC AF5667BR |
ControlCARD settings:
Certain settings on the device control card are required to communicate over JTAG and use the isolated UART port. The user must also provide a correct ADC reference voltage. The following settings are required for revision A of the TMS320F280049C control card (refer to the info sheet located at \c2000ware\boards\controlCARDs\TMDSCNCD280049C.