To quickly execute this build, follow the following steps:
- Make sure that all jumpers on the board are
correctly installed or removed as listed in the Hardware section.
- Hardware Set-up: Insert the F28004x controlCARD
in the 100-pin DIMM connector. Connect a 12 V DC bench power supply between TP10
and TP11 with correct polarity. Connect an isolated 400V programmable DC power
source to the 400 V input connector and 12 V electronic load to the 12 V
connector (make sure that this load does not exceed the board ratings). Connect
a USB cable between the PC and controlCARD. Do not turn ON any of the power
supplies at this time.
- Open Code Composer Studio. Maximize Code Composer Studio to fill your screen. Close the welcome screen if it opens up.
- locate the solution package downloaded and import the project in CCS
- In the project window on the left, click the plus sign (+) to the left of Project. Your project window will look like the following: