JAJU833 November   2021 AWR2944

 

  1.   概要
  2.   リソース
  3.   特長
  4.   アプリケーション
  5.   5
  6. 1System Description
    1. 1.1 Why use Radar?
    2. 1.2 TI Corner Radar Design
    3. 1.3 Key System Specification
  7. 2System Overview
    1. 2.1 Block Diagram
    2. 2.2 Design Considerations
    3. 2.3 Highlighted Products
      1. 2.3.1 AWR2944 Single-Chip Radar Solution
      2. 2.3.2 AWR2944 Evaluation Module
    4. 2.4 System Design Theory
      1. 2.4.1  Antenna Configuration
      2. 2.4.2  Chirp Configuration and System Performance
      3. 2.4.3  Data Path
      4. 2.4.4  Chirp Timing
      5. 2.4.5  eDMA Configuration
      6. 2.4.6  Memory Allocation
      7. 2.4.7  DDMA
      8. 2.4.8  Empty Subband Based DDMA
      9. 2.4.9  RANSAC
      10. 2.4.10 Group Tracker
  8. 3Hardware, Software, Testing Requirements, and Test Results
    1. 3.1 Required Hardware and Software
      1. 3.1.1 Hardware
      2. 3.1.2 Software and GUI
    2. 3.2 Test Setup
    3. 3.3 Test Results
  9. 4Design and Documentation Support
    1. 4.1 Design Files
      1. 4.1.1 Schematics
      2. 4.1.2 BOM
    2. 4.2 Tools and Software
    3. 4.3 Documentation Support
    4. 4.4 サポート・リソース
    5. 4.5 Trademarks
  10. 5About the Author

Group Tracker

Real world radar targets (cars, pedestrians, and so forth) are presented to a tracking processing layer as a set of multiple reflection points. Those detection points form a group of correlated measurements with range, angle, SNR, and radial velocity. The group tracker, tracks a cluster of points (also known as group) in 2D over time based on a constant acceleration motion model. Figure 2-11 shows the main functional blocks of the group tracker algorithm. The subblocks shown in white are classical extended Kalman filter (EKF) operations. The subblocks shown in orange are additions to support multipoint grouping. More details about the group tracking algorithm are found in Group Tracker Parameter Tuning Guide for the 3D People Counting Demo.


GUID-20211110-SS0I-KNSQ-DGBT-BXM9KWXLMJDP-low.gif

Figure 2-11 Group Tracker Block Diagram

These parameter sets can be tweaked based on test results or as per scene requirement.

Table 2-3 GTrack Parameter Sets
SCENARIO PARAMETER SETS CLI COMMANDS DESCRIPTION
1 Scenery Parameters appSceneryParams

These define the dimensions of the physical space in which the tracker will operate. These also specify the radar sensor orientation and position.

Any measurement points outside these boundary boxes are not used by the tracker.
2 Gating Parameters appGatingParams

These determine the maximum volume and velocity of a tracked object and are used to associate measurement points with tracks that already exist.

Points detected beyond the limits set by these parameters are not included in the set of points that make up the tracked object.
3 Allocation Parameters appAllocParams These are used to detect new tracks or people in the scene. When detected points are not associated with existing tracks, allocation parameters are used to cluster these remaining points and determine if that cluster qualifies as a person or target.
4 State Parameters appStateParams The state transition parameters determine the state of a tracking instance. Any tracking instance can be in one of three states: FREE, DETECT, or ACTIVE.
5

Max Acceleration Parameters

Max number of points

Max number of tracks

gtrack Max acceleration parameters determine the maximum acceleration in the lateral, longitudinal, and vertical directions.