JAJU833 November 2021 AWR2944
TX channels can be coded to introduce empty-bands in the Doppler spectrum. This allows more robust velocity disambiguation and Doppler-bin to TX-channel mapping in DDMA. To introduce two empty Doppler subbands, the phase added to each TX channel is modified as . Figure 2-8 and Figure 2-9 show the range-Doppler plane with = 4 and two empty-bands. The locations of these empty Doppler subbands are used to find the hypothesis that will determine the correct TX channel mapping and allow velocity disambiguation as shown in Figure 2-10.