JAJU835 December 2021
LED | PURPOSE |
---|---|
D1 | This LED is connected to the output of U1. The LED is turned ON when the output is asserted low and turned OFF when the output is asserted high. |
D2 | This LED is connected to the output of U2. The LED is turned ON when the output is asserted low and turned OFF when the output is asserted high. |
D3 | This LED is connected to the output of U3. The LED is turned ON when the output is asserted low and turned OFF when the output is asserted high. If U3 detects an external magnetic field, this LED is turned ON. |
D4 | This LED is connected to the output of U4. The LED is turned ON when the output is asserted low and turned OFF when the output is asserted high. If U4 detects an external magnetic field, this LED is turned ON. |
D5 (labeled LPWR on board) | This LED is connected to the VCC pin of the DRV5056 and provides info if the system is in sleep or active mode. The system is only in active mode if LEDs D1 and D2 are ON while LEDs D3 and D4 are OFF. |
D6 (labeled TRIG on board) | This LED changes its brightness based on how far the trigger is pressed. The further the trigger is pressed, the brighter this LED. |
DESIGNATOR | BOARD LABEL | PURPOSE |
---|---|---|
TP1 |
VCC |
Main power supply of the board. This is either connected to the TPS709 output or the positive terminal of the battery placed in the battery holder. |
TP2, TP3, TP4, TP13 |
GND |
Board GND |
TP5 |
SW1 |
Output of switch U1 |
TP6 |
SW2 |
Output of switch U2 |
TP7 |
VCC_2 |
VCC pin of DRV5056. When the trigger is not pressed, this is disconnected from VCC (test point TP1) on the board. When the trigger is pressed, VCC_2 is connected to VCC through the TPS22917 load switch. |
TP8 |
LIN |
Output of DRV5056 |
TP9 |
AMP |
Output of TLV9061, which drives the cathode of the TRIG (L6) LED so that it changes its brightness based on how far the trigger is pressed. |
TP10 |
DIV |
If R10 and R11 are used to divide the output voltage from the DRV5056, this is the divided down voltage. By default, the voltage divider is not enabled. To enable it, the op-amp circuit must be disabled by removing resistor R5 from the board. |
TP11 |
SW4 |
Output of switch U4 |
TP12 |
SW3 |
Output of switch U3 |
TP14 |
VIN |
LDO input. When the board is powered from an external power supply, this test point is connected to the external 5-V to 30-V power supply so it can regulate the voltage to 3.3 V. |
TP15 |
BV |
Connected to the voltage that you want enable signal option 2 to be referenced with respect to. This can be connected to the cordless power tool battery so that enable signal is referenced with respect to the high voltage. By default, the enable signal option 2 is not available due to this circuit not being populated. |
TP16 |
BO |
Enable signal option 2. By default, the enable signal option 2 is not available due to this circuit not being populated. If the system is in active mode, the voltage here is equal to BV. If the system is in sleep mode, the voltage here is at 0 V. |
TP17 |
LOGIC |
Enable signal option 1. This is taken from the SN74HCS00 output. This is available by default. If the system is in active mode, this test point is at 0 V. If the system is in sleep mode, the voltage of this test point is set to the VCC voltage. |