JAJU873 August   2020

 

  1.   概要
  2.   リソース
  3.   特長
  4.   アプリケーション
  5.   5
  6. 1 System Description
    1. 1.1 Medical Respiratory Systems
    2. 1.2 Respirator System Components
    3. 1.3 Key System Specifications
  7. 2System Overview
    1. 2.1 Block Diagram
    2. 2.2 Design Considerations
      1. 2.2.1 Brushless DC Motor (BLDC)
        1. 2.2.1.1 DRV8323RS BLDC Motor Driver Design Calculations
        2. 2.2.1.2 BLDC Motor Driver Circuit
      2. 2.2.2 Solenoid Valve Drivers
        1. 2.2.2.1 DRV8847 Solenoid Driver Design Calculations
        2. 2.2.2.2 Solenoid Driver Circuit
      3. 2.2.3 Power Tree Architecture
        1. 2.2.3.1 Input protection - overvoltage and reverse voltage
        2. 2.2.3.2 LM5122 Boost Design Calculations
        3. 2.2.3.3 LMR33630 Buck Design Calculations
        4. 2.2.3.4 Secondary Power Stage – TPS62840 3.3V Buck
        5. 2.2.3.5 Secondary Power Stage – TPS7A02 3.3V LDO
        6. 2.2.3.6 Power Tree Circuit
    3. 2.3 Highlighted Products
  8. 3Hardware, Software, Testing Requirements, and Test Results
    1. 3.1 Hardware and Software Requirements
    2. 3.2 Test Setup
      1. 3.2.1 Hardware Configuration
      2. 3.2.2 Software Configuration
    3. 3.3 Test Results
      1. 3.3.1 Motor Test Result
      2. 3.3.2 Valve Test Result
      3. 3.3.3 Power Tree Test Result
      4. 3.3.4 Key Test Summary
  9. 4Design and Documentation Support
    1. 4.1 Design Files
      1. 4.1.1 Schematics
      2. 4.1.2 BOM
    2. 4.2 Documentation Support
    3. 4.3 サポート・リソース
    4. 4.4 Trademarks
  10. 5About the Author

LMR33630 Buck Design Calculations

Based on the key system specification, the maximum solenoid load is 1.7 A. The boost-buck DC-DC power stage, consisting of LM5211 and LMR33630, is designed to support 2 A of continuous load. Note, WEBENCH® Power Designer was used to help design the power stage. The key design calculations for the LMR3360 Buck Stage are shown below. For more details on design considerations, please refer to the device data sheet.

Table 2-5 Buck stage summary
PARAMETER SPECIFICATION COMMENTS
Input Voltage 14-28 V From boost stage
Input Power 26.7 W Max, η = 90%
Output Voltage 12 V For solenoid drive
Output Power 24 W Max
Max Load Current 2 A Vout = 12 V (24 W)

The choice of switching frequency is a compromise between conversion efficiency and overall solution size. For this design, 400 kHz was chosen (i.e. LMR33630A variant) as a compromise between efficiency and overall solution size.

Setting the Output Voltage

The output voltage of the LMR33630 is externally adjustable using a resistor divider network. The target output is 12 V. Start with the recommended 100 kΩ value. The RFBB is:

Equation 84. GUID-20200804-CA0I-CWSQ-KZ3J-N0JLKMT6KSLG-low.gif

9.1 kΩ was selected.

Inductor Selection

The first step to calculate the peak inductor/switch current is to determine the duty cycle, D, for the maximum input voltage. The maximum input voltage is used because this leads to the maximum switch current:

Equation 85. GUID-20200804-CA0I-0JSM-VTR0-99S5DPM2WPTW-low.gif

The parameters for selecting the inductor are the inductance and saturation current. The inductance is based on the desired peak-to-peak ripple current and is normally chosen to be in the range of 20-40 % of the maximum output current. Note that when selecting the ripple current for applications with much smaller maximum load (2 A) than the maximum available from the device (3 A), the maximum device current should be used.

Equation 86. GUID-20200804-CA0I-QPWT-CH31-ZPTLHLJNPL7X-low.gif

The maximum inductance is limited by the minimum current ripple required for the current mode control to perform correctly. As a rule-of thumb, the minimum inductor ripple current must be no less than about 10% of the device maximum rated current under nominal conditions:

Equation 87. GUID-20200804-CA0I-0X8L-TN87-VBWHLWMLLDM0-low.gif

From the data sheet, the minimum inductance is given by:

Equation 88. GUID-20200804-CA0I-0QTM-0GQN-ZXGPVNKGZS5C-low.gif

RR of 0.3 was selected for the following inductance calculation:

Equation 89. GUID-20200804-CA0I-HGDV-N0SG-LGNH49ZS2D14-low.gif

For this design 33 μH was selected. This value is inside the recommended inductance range. Alternatively, a smaller inductance 22 μH (SPM7054VT-220M-D) could be used since the saturation current rating would be higher.

The actual worst-case ripple current is:

Equation 90. GUID-20200804-CA0I-4DGK-MTS6-DPH2TX6WGFPQ-low.gif

The actual ripple ratio is:

Equation 91. GUID-20200804-CA0I-HNWN-FRBN-X6331S2QT7QT-low.gif

The peak inductor/switch/diode current and the minimum saturation current rating of the inductor plus a 25% margin are calculated as follows:

Equation 92. GUID-20200804-CA0I-X5KZ-ZNWW-GVPZPT8S5L3C-low.gif

However, the LM33630 has specific inductor saturation requirement for its normal operation due to internal current limits. Ideally, the saturation current rating of the inductor must be at least as large as the high-side switch current limit, ISC. The ISC is 4.5 A typical and 5 A max.

In any case, the inductor saturation current must not be less than the device low-side current limit, ILIMIT. The ILIMIT is 3.5 A typical and 4.1 A max.

In this design, the selected inductor (SPM7054VT-330M-D) has saturation ratings of 3.6 A (ΔL=-20%) and 4.9 A ΔL=-30%). Based on the data sheet, this inductor RMS rating is well suited to handle 3.4 A with a 40 oC rise.

For the RMS current calculations, the 2 A max application current is used instead of the device maximum:

Equation 93. GUID-20200804-CA0I-L0T5-DS7D-CSDCWRDFDJZB-low.gif

Note, IRMS is approximately Iout given a small RR value.

Inductor wire loss is calculated as follows:

Equation 94. GUID-20200804-CA0I-R4DR-ZWCF-SP4LVZ5FKJVF-low.gif

Output Capacitor Selection

The value of the output capacitor and the ESR of the capacitor determine the output voltage ripple and load transient performance. The output capacitor bank is usually limited by the load transient requirements, rather than the output voltage ripple. The following equations can be used to estimate a lower bound on the total output capacitance and an upper bound on the ESR, which is required to meet a specified load transient. Assume a 2 A transient step with 5% voltage drop (600 mV), using the worst-case input:

Equation 95. GUID-20200804-CA0I-LGNJ-ZDBB-D5D4TRHXHJBQ-low.gif
Equation 96. GUID-20200804-CA0I-WSH6-6KCR-61MFHJVND9DJ-low.gif

In this design, three 22-μF and one 1-μF were used, which accounts for tolerance and voltage derating. These ceramic caps are rated for 25 V, so the de-rated output capacitance is 32 μF. Ceramic capacitors can easily meet the minimum ESR requirements. Assume an effective ESR of 50 mΩ for the ripple voltage calculations.

The peak-to-peak output voltage ripple is:

Equation 97. GUID-20200804-CA0I-V40L-JFLK-BSP2KLMXKS31-low.gif

The output cap RMS current is:

Equation 98. GUID-20200804-CA0I-LJNK-NZKR-PXKGFKCJ14K3-low.gif

Input Capacitor Selection

The ceramic input capacitors provide a low impedance source to the regulator in addition to supplying the ripple current and isolating switching noise from other circuits. A minimum of 10 µF of ceramic capacitance is required on the input of the LMR33630. This must be rated for at least the maximum input voltage (28 V). For this design, 10-µF and 220-nF ceramic caps were selected. Both capacitors are rated at 50 V, which accounts for voltage-derating.

The input cap RMS current is:

Equation 99. GUID-20200804-CA0I-XX70-G3WW-CSHCMLTSRLFF-low.gif

CBOOT

The LMR33630 requires a bootstrap capacitor connected between the BOOT pin and the SW pin. This capacitor stores energy that is used to supply the gate drivers for the power MOSFETs. For this design, a 100-nF, 50-V ceramic cap was selected based on the data sheet guidelines.

VCC

The VCC pin is the output of the internal LDO used to supply the control circuits of the regulator. This output requires a 1-µF, 16-V ceramic capacitor connected from VCC to GND for proper operation.

CFF Selection

In some cases, a feedforward capacitor can be used across RFBT to improve the load transient response or improve the loop-phase margin:

Equation 100. GUID-20200804-CA0I-VSNB-KBJR-FRMN8J6R29CQ-low.gif
Equation 101. GUID-20200804-CA0I-0TQ9-8BX5-MMW2WWKRF6CQ-low.gif

In this design, the CFF is DNP (Do Not Populate).

UVLO

This is not applicable for this stage of the power tree since it was implemented in the boost stage. If specific UVLO is required, refer to the LMR33630 data sheet for more information.

Maximum Ambient Temperature

The power dissipation is approximated with:

Equation 102. GUID-20200806-CA0I-XDTD-XF8M-DMGDZJWPDMSR-low.gif

Assume a 90% efficiency (Vin = 28 V) at max load:

Equation 103. GUID-20200806-CA0I-DDS3-FFJP-SJB3P4JWXWSR-low.gif

Assume a RθJA of 40 oC/W:

Equation 104. GUID-20200806-CA0I-BH2N-4R9S-SVT2LN1J4KZC-low.gif