JAJU873 August 2020
The following valve tests were conducted:
DRV8847 Valve Turn-On Time
The valve turn-on transition (<400 ns) is clean with minimal overshoot as shown in channel 1 in Figure 3-19.
DRV8847 Valve Turn-Off Time
The valve turn-off transition (<400ns) is clean with minimal overshoot as shown in channel 1 in Figure 3-20.
DRV8847 Consecutive Valve Operation
The transition between valves is clean with no overshoot as shown in channel 1 and 2 in Figure 3-21. Valve is seen and heard to engage during both events.
DRV8847 Bidirectional Valve Operation
The voltage waveforms for each side matched as shown in channel 1 and 2 in Figure 3-22. The observed current draw was the same for either direction. The valve is seen and heard to engage during both events.