JAJU878 November 2022 ADS117L11 , ADS127L11
The board can run from 2.5-V up to 3.3-V digital supply (a 1.8-V supply also works with the diagnostic features unavailable, D1 does not turn on in that case). Use 2.5 V for signal integrity, EMC, and power consumption reasons.
The board is designed to use the PHI digital supply by default when connected. In that mode:
Digital power supply at different speeds of ADC can be measured by attaching an ammeter on J6 instead of short.
If the external power supply is used:
If power supply is active, D1 is on.
The estimated current from the digital supply is below 30 mA.