SBAA621 March   2024 AFE20408

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Application Figure
  6. 3Output Configurations
  7. 4Power Sequencing
    1. 4.1 Power Up Positive Range
    2. 4.2 Power Up Negative Range
  8. 5Summary
  9. 6References

Power Up Negative Range

The power up for the negative range is similar to the positive range, but the outputs are tied to the VSS voltage during start-up. Figure 4-2 shows the start-up behavior. This means that during start-up there is a period where the outputs are within the on range of the PA. Because the PA can possibly be powered, the PA should be isolated from PAVDD so the PA does not erroneously turn on.

GUID-20240108-SS0I-QJ3J-0W4B-9SN3J6LXQ8SN-low.svgFigure 4-2 AFE20408 Negative Startup