SBAS771C June 2017 – February 2020
PRODUCTION DATA.
If a full-scale input signal is applied to the AMC1303 (that is, |VIN| ≥ |VClipping|), Figure 49 shows that the device generates a single one or zero every 128 bits at DOUT, depending on the actual polarity of the signal being sensed. In this way, differentiating between a missing AVDD and a full-scale input signal is possible on the system level.