SBAS895B May 2018 – April 2020
PRODUCTION DATA.
In frequency inverter applications, the power switches must be protected in case of an overcurrent condition. To allow for fast powering off of the system, a low delay caused by the isolated amplifier is required. Figure 53 shows the typical full-scale step response of the AMC1300. Consider the delay of the required window comparator and the micro contol unit (MCU) to calculate the overall response time of the system.
The high linearity and low temperature drift of offset and gain errors of the AMC1300, as shown in Figure 54, allow design of motor drives with low torque ripple.