SBAU206B april 2015 – may 2023 ADS1262 , ADS1263
The default ADC power-supply voltages (DVDD and AVDD) are generated by the PHI controller using power from the USB. The PHI provides 3.3-V and 5.5-V power rails. The 3.3-V power rail directly supplies the ADC DVDD voltage. The 5.5-V power rail is supplied to the input of the TPS7A4700, a low-noise, configurable-output LDO, to supply AVDD. The LDO output voltage depends on the internal reference voltage (VLDO_REF) of 1.4 V and the pin connections. Grounding any LDO pin between pin 4 through pin 12 adds that pin voltage to VLDO_REF and increases the LDO output voltage, LDOVOUT. Figure 5-1 shows that the ADS1263EVM grounds pin 6 and pin 10 (3P2V and 0P4V, respectively) to set LDOVOUT to 5 V.
Figure 5-1 also shows that the 5V_LDO output is used for the AVDD connections across the EVM. Additionally, the user can measure the AVDD current by connecting an ammeter between pins 1 and 2 of JP1 or the DVDD current by connecting an ammeter between pins 1 and 2 of JP3.
External power sources can also be provided for each supply voltage:
When using either internal or external power supplies, LEDs D2 and D3 indicate if power is connected to AVDD and DVDD, respectively. These LEDs do not necessarily indicate if AVDD is 5 V or if DVDD is 3.3 V. Check the AVDD voltage using terminal JP6:1 and check the DVDD voltage using test point TP9. Figure 5-2 shows the portion of the schematic that includes the AVDD and DVDD LEDs.