SBAU206B april 2015 – may 2023 ADS1262 , ADS1263
Figure 7-3 shows that the EVM global controls are located on the left side of the GUI. These controls include the filter type, data rate, PGA gain, input channels, number of samples, and others. The Pages control in the upper-left allows access to the other pages in the GUI. Figure 7-3 also shows the ADC register settings. The registers can be used to set the different device modes such as power, PGA, and ADC selection. Change the register settings by clicking on each bit, typing a value directly into the Value column, or by selecting from the drop-down menus in the Field View control.