After installing the EVM software, connect the EVM
as shown in Figure 7-1 and as described in the following steps:
- Physically connect P2 of the PHI to J1 of the ADS1263EVM. Install the screws to provide a robust connection.
- Connect the USB cable from the computer to the PHI.
- LED D5 on the PHI lights up, indicating that the PHI is powered up.
- LEDs D1 and D2 on the PHI start blinking to
indicate that the PHI is booted up and communicating with the PC. Figure 7-1 shows the resulting LED indicators.
- Start the software GUI as shown in Figure 7-2. The LEDs blink slowly as the FPGA firmware is loaded on the PHI. This
loading takes a few seconds and then the AVDD and DVDD power supplies turn on,
as indicated by LEDs D1, D2, and D3 on the ADS1263EVM.
- Connect external sensors to terminal blocks J3-J6
in accordance with the examples given in Section 3.1.2.