SBAU260 April 2016
The activity log is the control that consumes most of the display located in the lower half of the window. This shows any messages, USB activity, and communication that may be of interest. The Options menu allows for the customization of message-level display in the activity log. See Section 5.3 for more details.
The activity log has a small context menu that can be accessed by right-clicking on the activity log. Select Clear Log Screen or Clear Log to perform the desired function to the log. Clear Log Screen only clears the contents of the activity log display and does not clear the log history. Clear Log clears the entire log history. Once the log is cleared, only log items from this point forward can be viewed using the Master Log Viewer (see Section 10).