SBAU260 April 2016
This control shows a list of the commands that are available for use in the script. Selecting an item in this list populates the Command Message control with the selected command and corresponding help.
NOTE
If the command requires additional arguments, they need to be added to the Command Message control after the command is selected.