SBAU260 April 2016
This option enables the user to change controls for the register settings without creating a register write or update after every control change. Once all the settings within the register are configured to the user's specifications, a manual write command must be issued using the Write Selected Register button that appears once this option is enabled on the Device tab.
NOTE
Without the manual button press, the values in the register map table reflect changes but the device hardware is not synchronized to these values.