SBAU321B November 2018 – June 2021 ADS7142 , ADS7142-Q1
In the Autonomous Conversion Mode, the device generates the start of conversion pulses using an internal oscillator on receiving the first start of conversion pulse from the host. This can be configured by selecting Autonomous Mode as the Conversion Mode, selecting one of the Operating Modes from the drop-down menu, and pressing the SET button. The ADS7142-Q1 device then generates the subsequent start of conversion signals autonomously. The Operating Modes offered in Autonomous Mode are described in the following sections.